MCUXpresso SDK Documentation

ZPS_tsAfNwkRouteDiscoveryConfEvent

ZPS_tsAfNwkRouteDiscoveryConfEvent#

This structure is used in the ZPS_EVENT_NWK_ROUTE_DISCOVERY_CONFIRM event, which confirms that a route discovery has been performed.

The ZPS_tsAfNwkRouteDiscoveryConfEventstructure is detailed below.

typedef struct {
    uint16 u16DstAddress;
    uint8 u8Status;
    uint8 u8NwkStatus;
} ZPS_tsAfNwkRouteDiscoveryConfEvent;

where:

  • u16DstAddressis the destination address for which the route discovery confirm event was generated.

  • u8Statusis one of the status codes from the MAC layer, detailed in Section11.2.4.

  • u8NwkStatusis one of the status codes from the NWK layer, detailed in Section 11.2.3.

Parent topic:Event structures