MCUXpresso SDK Documentation

ZPS_tsAfNwkLeaveIndEvent

ZPS_tsAfNwkLeaveIndEvent#

This structure is used in the ZPS_EVENT_LEAVE_INDICATION event, which indicates that a neighboring node has left the network or a remote node has requested the local node to leave.

The ZPS_tsAfNwkLeaveIndEventstructure is detailed below.

typedef struct {
    uint64 u64ExtAddr;
    uint8 u8Rejoin;
} ZPS_tsAfNwkLeaveIndEvent;

where:

  • u64ExtAddris the 64-bit IEEE (MAC) address of the node that has left the network, or is zero if the local node has been requested to leave the network

  • u8Rejoinindicates whether the leaving node was requested to attempt a subsequent rejoin of the network:

    • zero represents FALSE

    • a non-zero value represents TRUE.

Parent topic:Event structures