MCUXpresso SDK Documentation

ZPS_tsAfNwkJoinFailedEvent

ZPS_tsAfNwkJoinFailedEvent#

This structure is used in the event ZPS_EVENT_NWK_FAILED_TO_JOIN, which indicates that the local device has failed to join a network.

The ZPS_tsAfNwkJoinFailedEventstructure is detailed below.

typedef struct
{
    uint8 u8Status;
    bool_t bRejoin;
} ZPS_tsAfNwkJoinFailedEvent;

where:

  • u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.

  • bRejoinindicates whether the join attempt was a rejoin (TRUE) or a new association (FALSE).

Parent topic:Event structures