MCUXpresso SDK Documentation

ZPS_tsAfNwkEdScanConfEvent

ZPS_tsAfNwkEdScanConfEvent#

This structure is used in the ZPS_EVENT_NWK_ED_SCAN event, which indicates that an ‘energy detect’ scan in the 2.4-GHz radio band is completed.

The ZPS_tsAfNwkEdScanConfEventstructure is defined as:

typedef ZPS_tsNwkNlmeCfmEdScan ZPS_tsAfNwkEdScanConfEvent;

where ZPS_tsNwkNlmeCfmEdScanis described in Section 8.2.3.2.

Parent topic:Event structures