MCUXpresso SDK Documentation

ZPS_tsNwkNlmeCfmEdScan

ZPS_tsNwkNlmeCfmEdScan#

This structure is used by the structure ZPS_tsAfNwkEdScanConfEvent, which is created as part of the ZPS_EVENT_NWK_ED_SCAN event which reports the results of an ‘energy detect’ scan in the 2.4-GHz radio band.

The ZPS_tsNwkNlmeCfmEdScantstructure is detailed below.

typedef struct
{
    uint8 u8Status;
    uint8 u8ResultListSize;
    uint8 au8EnergyDetect[ZPS_NWK_MAX_ED_RESULTS];
} ZPS_tsNwkNlmeCfmEdScan;

where

  • u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.

  • u8ResultListSizeis the number of entries in the results list (see below).

  • au8EnergyDetect[]is an array containing the list of results of the energy scan (8-bit values representing the detected energy levels in the channels). There is one array element for each channel scanned, where element 0 is for the first channel scanned, element 1 is for the second channel scanned, etc.

Parent topic:Other structures