MCUXpresso SDK Documentation

ZPS_tsAfNwkDiscoveryEvent

ZPS_tsAfNwkDiscoveryEvent#

This structure is used in the ZPS_EVENT_NWK_DISCOVERY_COMPLETE event, which reports the details of the networks detected in a network discovery initiated by a Router or End Device that needs to join a network.

The ZPS_tsAfNwkDiscoveryEventstructure is detailed below.

typedef struct
{
    uint32        u32UnscannedChannels;
    uint8         eStatus;
    uint8         u8NetworkCount;
    uint8         u8SelectedNetwork;
    ZPS_tsNwkNetworkDescr *psNwkDescriptors;
} ZPS_tsAfNwkDiscoveryEvent;

where:

  • u32UnscannedChannelsis a 32-bit bitmap representing the set of channels from the network discovery that had not yet been scanned when this event was generated. Bits 11 to 26 represent the 2400-MHz channels 11 to 26, where 1 indicates channel scanned and 0 indicates channel not yet scanned.

  • estatusis the status of the network discovery process, returned by the lower layers (see Section 11.2) - MAC_ENUM_SUCCESS, if the discovery was successfully completed.

  • u8NetworkCountis the number of networks that had been discovered when this event was generated.

  • u8SelectedNetworkis the index of the recommended network in the array of reported networks (see below).

  • psNwkDescriptorsis a pointer to the network discovery table in the network NIB. The network discovery table contains an array of data structures, where each structure contains details of a discovered network. Each array element is a structure of the type ZPS_tsNwkNetworkDescr, described in Section 8.2.3.1. The number of array elements is given by u8NetworkCount, described above.

Parent topic:Event structures