ZPS_eAplZdoDiscoverNetworks
ZPS\_teStatus ZPS\_eAplZdoDiscoverNetworks\(uint32 u32ChannelMask\);
Description
This function can be used by a Router or End Device to initiate a network discovery
that is, to find a network to join.
A network discovery is performed when the stack is started using the function ZPS_eAplZdoStartStack(). The function ZPS_eAplZdoDiscoverNetworks() can be used to perform subsequent network discoveries (for example, if the initial search did not yield any suitable networks).
As part of this function call, you must specify a value which indicates the 2400-MHz radio channels (numbered 11 to 26) to be used in the network search. There are two ways of setting this parameter:
A single value in the range 11 to 26 can be specified, indicating that the corresponding channel (and no other) must be used - for example, 12 indicates use channel 12.
A 32-bit mask can be used to specify a set of channels that the device will scan to find a network - each of bits 11 to 26 represents the corresponding radio channel, where the channel will be included in the scan if the bit is set to 1 (and excluded if cleared to 0). Therefore, the value 0x07FFF800 represents all channels.
Note: If an invalid value is specified for this parameter, the default value of 0x07FFF800 (all channels) will be used.
If this function successfully initiates a network discovery, ZPS_E_SUCCESS will be returned. The network discovery results will then be reported through the event ZPS_EVENT_NWK_DISCOVERY_COMPLETE (for details of this event, refer to Section 7.2.2.9). This includes a list of the detected networks and the index (in the list) of the recommended network to join. You should then call ZPS_eAplZdoJoinNetwork() to join the desired network.
Parameters
u32ChannelMask Radio channel(s) for network discovery (see above)
Returns
ZPS_E_SUCCESS (network discovery started)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:Network deployment functions