MCUXpresso SDK Documentation

ZPS_bAplZdoTrustCenterSetDevicePermissions

ZPS_bAplZdoTrustCenterSetDevicePermissions#

ZPS_teStatus
ZPS_bAplZdoTrustCenterSetDevicePermissions(
  uint64 u64DeviceAddr,
  ZPS_teTCDevicePermissions u8DevicePermissions);

Description#

This function can be used by the Trust Centre to set the permissions for certain requests from a particular node. The possible settings are:

  • Allow all requests from the specified node (ALL_PERMITED)

  • Do not allow join requests from the specified node (JOIN_DISALLOWED)

  • Do not allow data requests from the specified node (DATA_REQUEST_DISALLOWED)

Parent topic:ZPS_bAplZdoTrustCenterSetDevicePermissions

Parameters#

  • u64DeviceAddr: 64-bit IEEE/MAC address of node for which permissions are to be set

  • u8DevicePermissions: Bitmap of permissions to be set, constructed using the following enumerations:

    • ZPS_TRUST_CENTER_ALL_PERMITED

    • ZPS_TRUST_CENTER_JOIN_DISALLOWED

    • ZPS_TRUST_CENTER_DATA_REQUEST_DISALLOWED

Parent topic:ZPS_bAplZdoTrustCenterSetDevicePermissions

Returns#

  • ZPS_E_SUCCESS (permissions successfully set)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_bAplZdoTrustCenterSetDevicePermissions

Parent topic:Security functions