General ZPS Resources
The chapter describes the general API resources provided in the ZigBee PRO Stack (ZPS) software.
In this chapter:
The ZigBee Queue resources are detailed in Section 10.1.
The ZigBee Timer resources are detailed in Section 10.2.
The Critical Section and Mutex resources are detailed in Section 10.3.
Note: Amongst the general resources, functions are supplied to allow the extraction of payload data from received ZDP packets. These resources are not documented here but are provided in the header file appZdpExtractions.h.
ZigBee Queue Resources
The ZigBee Queue resources are concerned with creating and operating queues for passing messages from one task to another. These resources are provided in the header file ZQueue.h.
The ZigBee Queue functions are described in Section 10.1.1.
The ZigBee Queue structures are described in Section 10.1.2.
ZigBee queue functions
The ZigBee Queue functions are listed below.
Function page
Parent topic:ZigBee queue functions
ZQ_vQueueCreate
void ZQ_vQueueCreate(tszQueue *psQueueHandle,
const uint32 uiQueueLength,
const uint32 uiItemSize,
uint8 *pu8StartQueue);
Description
This function creates a message queue for use by the application or stack (message queues are described in Section 6.9.1). The size of the queue and the size of a message in the queue must be specified, as well as the location in memory where the queue should start. A unique handle must also be given to the queue, where this handle is a pointer to a tszQueuestructure that contains up-to-date information about the queue.
Parameters
psQueueHandle Handle of message queue - this is a pointer to a
tszQueuestructure (see Section 10.1.2.1).uiQueueLength Size of the queue in terms of the number of messages that it can hold.
uiItemSize Size of a message in the queue, in bytes.
pu8StartQueue Pointer to the start of the message queue.
Parent topic:ZQ_vQueueCreate
Returns
None
Parent topic:ZQ_vQueueCreate
Parent topic:ZigBee queue functions
ZQ_bQueueSend
bool_t ZQ_bQueueSend(void *pvQueueHandle,
const void *pvItemToQueue);
Description
This function submits a message to the specified message queue. The return code indicates whether the message was successfully added to the queue.
Parent topic:ZQ_bQueueSend
Parameters
pvQueueHandle Handle of message queue
pvItemToQueue Pointer to the message to be added to the queue
Parent topic:ZQ_bQueueSend
Returns
Boolean indicating the outcome of the operation:
TRUE - message successfully added to the queue
FALSE - message not added to the queue
Parent topic:ZQ_bQueueSend
Parent topic:ZigBee queue functions
ZQ_bQueueReceive
ZQ_bQueueReceive(void *pvQueueHandle,
void *pvItemFromQueue);
Description
This function obtains a message from the specified message queue. The return code indicates whether a message was successfully obtained from the queue.
Parent topic:ZQ_bQueueReceive
Parameters
pvQueueHandle: Handle of message queue
pvItemFromQueue: Pointer to memory location to receive the obtained message
Parent topic:ZQ_bQueueReceive
Returns
Boolean indicating the outcome of the operation:
TRUE - message successfully obtained from the queue.
FALSE - message not obtained from the queue.
Parent topic:ZQ_bQueueReceive
Parent topic:ZigBee queue functions
ZQ_bQueueIsEmpty
bool_t ZQ_bQueueIsEmpty(void *pvQueueHandle);
Description
This function checks whether the specified message queue is empty. The return code indicates whether the queue is empty.
Parent topic:ZQ_bQueueIsEmpty
Parameters
pvQueueHandle Handle of message queue
Parent topic:ZQ_bQueueIsEmpty
Returns
Boolean indicating the outcome of the operation:
TRUE - message queue is empty.
FALSE - message queue is not empty.
Parent topic:ZQ_bQueueIsEmpty
Parent topic:ZigBee queue functions
ZQ_u32QueueGetQueueSize
bool_t ZQ_bQueueIsEmpty(void *pvQueueHandle);
Description
This function obtains the capacity of the specified message queue. The return code indicates the size of the queue in terms of the number of messages that it can hold.
Parent topic:ZQ_u32QueueGetQueueSize
Parameters
pvQueueHandle Handle of message queue
Parent topic:ZQ_u32QueueGetQueueSize
Returns
The capacity of the queue in terms of the number of messages that it can hold.
Parent topic:ZQ_u32QueueGetQueueSize
Parent topic:ZigBee queue functions
ZQ_u32QueueGetQueueMessageWaiting
uint32 ZQ_u32QueueGetQueueMessageWaiting(
void *pu8QueueHandle);
Description
This function obtains the number of messages that are currently waiting in the specified message queue.
Parent topic:ZQ_u32QueueGetQueueMessageWaiting
Parameters
pvQueueHandle Handle of message queue
Parent topic:ZQ_u32QueueGetQueueMessageWaiting
Returns
Number of messages waiting in the queue
Parent topic:ZQ_u32QueueGetQueueMessageWaiting
Parent topic:ZigBee queue functions
Parent topic:ZigBee Queue Resources
ZigBee queue structures
tszQueue
The ZigBee queue structure tszQueueis shown below.
typedef struct
{
uint32 u32Length;
uint32 u32ItemSize;
uint32 u32MessageWaiting;
void *pvHead;
void *pvWriteTo;
void *pvReadFrom;
}tszQueue;
where:
u32Lengthis the size of the queue in terms of the number of messages that it can holdu32ItemSizeis the size of a message, in bytesu32MessageWaitingis the number of messages currently in the queuepvHeadis a pointer to the beginning of the queue storage areapvWriteTois a pointer to the next free place in the storage area where a new message can be writtenpvReadFromis a pointer to the next message to be read from the storage area
Parent topic:ZigBee queue structures
Parent topic:ZigBee Queue Resources
Parent topic:General ZPS Resources
ZigBee Timer resources
The ZigBee Timer functions are concerned with initializing and operating software timers. These resources are provided in the header file ZTimer.h.
The ZigBee Timer functions are described in Section 10.2.1
The ZigBee Timer structures are described in Section 10.2.2
ZigBee Timer functions
The functions are listed below.
Function page
To use the software timers, the while loop of your application must include a call to the following function:
void ZTIMER\_vTask\(void\);
Parent topic:ZigBee Timer functions
ZTIMER_eInit
ZTIMER_teStatus ZTIMER_eInit(ZTIMER_tsTimer *psTimers,
uint8 u8NumTimers);
Description
This function initializes a set of software timers for use by the application. A list of timers is provided in an array, in which each array element is a structure containing information on one timer (see Section 10.2.2.1). The index of an array element is used as a reference for the corresponding timer.
In order to use one of the initialized timers, it must first be opened using ZTIMER_eOpen().
Parent topic:ZTIMER_eInit
Parameters
psTimers: Pointer to an array of structures, where each array element contains information for one timer (see Section 10.2.2.1)
u8NumTimers: Number of timers in the above array
Parent topic:ZTIMER_eInit
Returns
E_ZTIMER_OK (timers successfully initialized)
E_ZTIMER_FAIL (timers not initialized)
Parent topic:ZTIMER_eInit
Parent topic:ZigBee Timer functions
ZTIMER_eOpen
ZTIMER_teStatus ZTIMER_eOpen(
uint8 *pu8TimerIndex,
ZTIMER_tpfCallback pfCallback,
void *pvParams,
uint8 u8Flags);
Description
This function is used to open the specified software timer. A list of parameter values for the timer must be provided as well as a user-defined callback function that will be used to perform any operations required on expiration of the timer.
The callback function has the following prototype:
typedef void (*ZTIMER_tpfCallback)(void * pvParam );
where pvParam is a pointer to the timer parameters.
The function also includes a parameter u8Flags, which specifies whether the timer should allow or prevent sleep. When activity checks are made to decide whether the device can enter sleep mode, the value of this flag determines if the (running) timer will stop the device from going to sleep.
Before a timer is opened, it must have been initialized in a call to ZTIMER_eInit().
Parent topic:ZTIMER_eOpen
Parameters
pu8TimerIndex Pointer to location containing the index number of the timer in the list of timers initialized using ZTIMER_eInit()
pfCallback Pointer to the user-defined callback function for the timer
pvParams Pointer to a list of parameter values for the timer u8Flags Flag indicating whether the timer should allow or prevent sleep, one of:
ZTIMER_FLAG_ALLOW_SLEEP
ZTIMER_FLAG_PREVENT_SLEEP
Parent topic:ZTIMER_eOpen
Returns
E_ZTIMER_OK (timer successfully opened)
E_ZTIMER_FAIL (timer not opened)
Parent topic:ZTIMER_eOpen
Parent topic:ZigBee Timer functions
ZTIMER_eClose
ZTIMER_teStatus ZTIMER_eClose(uint8 u8TimerIndex);
Description
This function is used to close the specified software timer when it is no longer needed. The timer must have been previously opened using ZTIMER_eOpen().
Parent topic:ZTIMER_eClose
Parameters
u8TimerIndex: Index number of the timer in the list of timers initialized using ZTIMER_eInit().
Parent topic:ZTIMER_eClose
Returns
E_ZTIMER_OK (timer successfully closed)
E_ZTIMER_FAIL (timer not closed - may be running or already closed)
Parent topic:ZTIMER_eClose
Parent topic:ZigBee Timer functions
ZTIMER_eStart
ZTIMER_teStatus ZTIMER_eStart(uint8 u8TimerIndex,
uint32 u32Time);
Description
This function is used to start the specified software timer. The length of time for which the timer will run must be specified in milliseconds.
Before a timer is started, it must have been opened using ZTIMER_eOpen(). Once started, the timer can be stopped (before it expires) using ZTIMER_eStop().
Parent topic:ZTIMER_eStart
Parameters
pu8TimerIndex: Index number of the timer in the list of timers initialized using ZTIMER_eInit().
u32Time: The time, in milliseconds, for which the timer should run.
Parent topic:ZTIMER_eStart
Returns
E_ZTIMER_OK (timer successfully started)
E_ZTIMER_FAIL (timer not started)
Parent topic:ZTIMER_eStart
Parent topic:ZigBee Timer functions
ZTIMER_eStop
ZTIMER_teStatus ZTIMER_eStop(uint8 u8TimerIndex);
Description
This function is used to stop the specified software timer (before it expires). The timer must have been previously started using ZTIMER_eStart().
Parent topic:ZTIMER_eStop
Parameters
pu8TimerIndex: Index number of the timer in the list of timers initialized using ZTIMER_eInit().
Parent topic:ZTIMER_eStop
Returns
E_ZTIMER_OK (timer successfully stopped)
E_ZTIMER_FAIL (timer not stopped - may be already stopped or expired)
Parent topic:ZTIMER_eStop
Parent topic:ZigBee Timer functions
ZTIMER_eGetState
ZTIMER_teStatus ZTIMER_eGetState(uint8 u8TimerIndex);
Description
This function is used to obtain the current state of the specified software timer. The possible reported states are:
Running
Stopped
Expired
Closed
Parent topic:ZTIMER_eGetState
Parameters
pu8TimerIndex Index number of the timer in the list of timers initialized using ZTIMER_eInit().
Parent topic:ZTIMER_eGetState
Parent topic:ZigBee Timer functions
Parent topic:ZigBee Timer resources
ZigBee timer structures
ZTIMER_tsTimer
The ZigBee timer structure is shown below. It is used to represent a single software timer that may be used by the application.
typedef struct
{
ZTIMER_teState eState;
uint32 u32Time;
void *pvParameters;
ZTIMER_tpfCallback pfCallback;
} ZTIMER_tsTimer;
where:
eStaterepresents the current state of the timer, as one of:E_ZTIMER_STATE_CLOSED
E_ZTIMER_STATE_STOPPED
E_ZTIMER_STATE_RUNNING
E_ZTIMER_STATE_EXPIRED
u32Timeis the remaining time, in milliseconds, that the timer still has to runpvParametersis a pointer to a set of parameters used by the timerpfCallbackis a pointer to the user-defined callback function that will be called when the timer expires - this function has the prototype:typedef void \(\*ZTIMER\_tpfCallback\)\(void \pvParam*\);
where
pvParamis a pointer to the timer parameters.
Parent topic:ZigBee timer structures
Parent topic:ZigBee Timer resources
Parent topic:General ZPS Resources
Critical Section and Mutex Resources
The Critical Section and Mutex functions are concerned with protecting sections of application code from preemption and re-entrancy. These resources are provided in the header file portmacro.h.
The Critical Section and Mutex functions are described in Section 10.3.1.
The Critical Section and Mutex structures are described in Section 10.3.2.
Critical Section and Mutex functions
The functions are listed below.
Function page
Parent topic:Critical Section and Mutex functions
ZPS_eEnterCriticalSection
uint8 ZPS_eEnterCriticalSection(
void *hMutex,
uint32* psIntStore);
Description
This function can be used to mark the end of a critical section of application code. The function ZPS_eEnterCriticalSection() must have been called at the start of the critical section.
This function can be used to mark the start of a critical section of application code - this is a code section that cannot be preempted by an interrupt with priority level less than 12. The function ZPS_eExitCriticalSection() must be called at the end of the critical section.
A pointer to a ‘priority level’ value must be provided, which contains the current priority level of the main application thread (when critical sections are not being executed). When a critical section is entered, the priority level of the main thread is increased such that interrupts with a priority of 11 or less cannot preempt the main thread. At the end of the critical section, the priority level of the main thread is returned to its value from before the critical section was entered.
Optionally, a mutex can also be applied during the critical section to protect the section from re-entrancy. If a mutex is required, a pointer must be provided to a user- defined mutex function with the following prototype:
((bool_t*) (*) (void))
This function must define and maintain a Boolean flag that indicates whether the corresponding mutex is active (TRUE) or inactive (FALSE). This flag is used by ZPS_eEnterCriticalSection() to determine whether the mutex is available.
If this flag reads as FALSE, the mutex is applied and the above mutex function must set the flag to TRUE.
If the flag is already TRUE, then the mutex cannot be applied - in this case, ZPS_eEnterCriticalSection() returns a failure.
Critical sections and mutexes are further described in Section 6.9.3.
Parent topic:ZPS_eEnterCriticalSection
Parameters
hMutex Pointer to user-defined mutex function (see above) - set to NULL if no mutex is required
psIntStore Pointer to structure containing ‘priority level’ value (see Section 10.3.2.1)
Parent topic:ZPS_eEnterCriticalSection
Returns
0x00 for success, 0x01 for failure (all other values are reserved)
Parent topic:ZPS_eEnterCriticalSection
Parent topic:Critical Section and Mutex functions
ZPS_eExitCriticalSection
uint8 ZPS_eExitCriticalSection(
void *hMutex,
uint32* psIntStore);
Description
This function can be used to mark the end of a critical section of application code. The function ZPS_eEnterCriticalSection() should be called at the start of the critical section.
A pointer to the ‘priority level’ value must be provided. If a mutex was used in the critical section, a pointer to the relevant mutex function must be provided in order to release the mutex.
Critical sections and mutexes are further described in Section 6.9.3.
Parent topic:ZPS_eExitCriticalSection
Parameters
hMutex Pointer to user-defined mutex function (see above) - set to
NULLif no mutex was used.psIntStore Pointer to structure containing ‘priority level’ value (see Section 10.3.2.1).
Parent topic:ZPS_eExitCriticalSection
Returns
0x00 for success, 0x01 for failure (all other values are reserved)
Parent topic:ZPS_eExitCriticalSection
Parent topic:Critical Section and Mutex functions
ZPS_u8GrabMutexLock
uint8 ZPS_u8GrabMutexLock(
void *hMutex,
uint32* psIntStore);
Description
This function can be used to apply a mutex at the start of a section of application code that is to be protected from re-entrancy. The function **ZPS_u8ReleaseMutexLock()**must be called at the end of the mutex-protected section to release the mutex.
A pointer must be provided to a user-defined mutex function with the following prototype:
((bool_t*) (*) (void))
This function must define and maintain a Boolean flag which indicates whether the corresponding mutex is active (TRUE) or inactive (FALSE). This flag is used by ZPS_u8GrabMutexLock() to determine whether the mutex is available. If this flag reads as FALSE, the mutex is applied and the above mutex function must set the flag to TRUE, but if the flag is already TRUE then the mutex cannot be applied - in the latter case, ZPS_u8GrabMutexLock() returns a failure.
A pointer to a ‘priority level’ value must be provided, which contains the current priority level of the main application thread (when mutex protection is not being implemented). When a mutex is applied, the priority level of the main thread is increased such that interrupts with a priority of 11 or less cannot preempt the main thread. When the mutex is released, the priority level of the main thread will be returned to its value from before the mutex was applied.
Mutexes are further described in Section 6.9.3.
Parent topic:ZPS_u8GrabMutexLock
Parameters
hMutex Pointer to user-defined mutex function (see above)
psIntStore Pointer to structure containing ‘priority level’ value (see Section 10.3.2.1).
Parent topic:ZPS_u8GrabMutexLock
Returns
0x00 for success, 0x01 for failure (all other values are reserved).
Parent topic:ZPS_u8GrabMutexLock
Parent topic:Critical Section and Mutex functions
ZPS_u8ReleaseMutexLock
uint8 ZPS_u8ReleaseMutexLock(
void *hMutex,
uint32* psIntStore);
Description
This function can be used to release a mutex that has been applied to a section of application code. The function ZPS_u8GrabMutexLock() must have been called at the start of the mutex-protected section.
A pointer to the relevant mutex function must be provided in order to release the mutex. A pointer to the ‘priority level’ value must also be provided.
Mutexes are further described in Section 6.9.3.
Parent topic:ZPS_u8ReleaseMutexLock
Parameters
hMutex Pointer to user-defined mutex function (see above).
psIntStore Pointer to structure containing ‘priority level’ value (see Section 10.3.2.1).
Parent topic:ZPS_u8ReleaseMutexLock
Returns
0x00 for success, 0x01 for failure (all other values are reserved)
Parent topic:ZPS_u8ReleaseMutexLock
Parent topic:Critical Section and Mutex functions
Parent topic:Critical Section and Mutex Resources
Critical Section and Mutex Structures
u32MicroIntStorage
u32MicroIntStorageis a 32-bit mask of the interrupts currently enabled. The u32MicroIntStoragestructure is used in critical sections and mutex-protected sections where u32MicroIntStoragetakes the interrupts that have been enabled.
Parent topic:Critical Section and Mutex Structures
Parent topic:Critical Section and Mutex Resources
Parent topic:General ZPS Resources