ZigBee timer structures
ZTIMER_tsTimer
The ZigBee timer structure is shown below. It is used to represent a single software timer that may be used by the application.
typedef struct
{
ZTIMER_teState eState;
uint32 u32Time;
void *pvParameters;
ZTIMER_tpfCallback pfCallback;
} ZTIMER_tsTimer;
where:
eStaterepresents the current state of the timer, as one of:E_ZTIMER_STATE_CLOSED
E_ZTIMER_STATE_STOPPED
E_ZTIMER_STATE_RUNNING
E_ZTIMER_STATE_EXPIRED
u32Timeis the remaining time, in milliseconds, that the timer still has to runpvParametersis a pointer to a set of parameters used by the timerpfCallbackis a pointer to the user-defined callback function that will be called when the timer expires - this function has the prototype:typedef void \(\*ZTIMER\_tpfCallback\)\(void \pvParam*\);
where
pvParamis a pointer to the timer parameters.
Parent topic:ZigBee timer structures
Parent topic:ZigBee Timer resources