Enabling RADE v1 Usage (non-LCE)#
Follow the steps below to disable LCE acceleration support and use the RADE v1 algorithm instead of the default RADE v2.
Open
/examples/_boards/ /wireless_examples/bluetooth/<example_name>/prj.conf:
replace CONFIG_MCUX_COMPONENT_middleware.wireless.rade2_algo_cm33_lce_lib=y with CONFIG_MCUX_COMPONENT_middleware.wireless.rade1_algo_cm33_lib=y.
replace CONFIG_MCUX_PRJSEG_module.board.wireless.linker_script_ble_loc=y with CONFIG_MCUX_PRJSEG_module.board.wireless.linker_script_ble=y
disable CONFIG_MCUX_PRJSEG_module.board.wireless.app_lce
Running the RADE algorithm without LCE support increases stack size requirements. Ensure the stack size for the task on which the algorithm runs is at least 3300 octets.
Note: Make sure the above components are listed only once in the prj.conf file. If duplicates exist, remove them before building the project.