MCUXpresso SDK Documentation

Brief Driver-Only Configuration Guide#

In-depth guide#

For more comprehensive and up-to-date information on driver-only builds, please refer to the /middleware/mbedtls3x/docs/driver-only-builds.md document.

Mbed TLS 3.x#

Default config file at : mbedtls3x/include/mbedtls/mbedtls_config.h

To use, keep these steps in mind#

  • This config is always enabled and should not be bypassed.

  • Define MBEDTLS_CONFIG_FILE with your config filename to use your own configuration file instead of the default one.

  • Disable all MBEDTLS_xxx_C algorithm macros that you do not want the software implementations of. Disabling them makes the build system skip the Mbed TLS 3.x built-in implementations (NOTE: READ IMPORTANT CAVEAT BELOW).

Caveat for MBEDTLS_xxx_C#

These macros may get re-enabled automatically by the config_adjust_legacy_*.h reconfig files if the disabled feature macro is a dependency for another.

This mainly relates to PSA-based configurations (see the PSA section below). If you PSA_WANT some algorithm and not all prerequisites for that algorithm are MBEDTLS_PSA_ACCELerated, then the appropriate MBEDTLS_xxx_C macros will get enabled automatically by the config_adjust_legacy_from_psa.h reconfig file.

In short, PSA_WANT has higher priority over MBEDTLS_xxx_C.

PSA#

Default config file at : mbedtls3x/include/psa/crypto_config.h

To use, keep these steps in mind#

  • MBEDTLS_PSA_CRYPTO_CONFIG must be enabled to use the PSA_WANT macros (see below). This option needs to be enabled in the Mbed TLS 3.x config file (disabled by default; you can find it commented out in mbedtls_config.h).

  • Define MBEDTLS_PSA_CRYPTO_CONFIG_FILE with your config filename to use your own configuration file instead of the default one.

  • Enable all the PSA_WANT macros in this config file that are required for your project. Granularity is fairly fine-grained, but not atomic (e.g. no distinguishing between one-go and multipart operations). This macro just enables the functionality that you PSA_WANT. This means that functionality may be provided either by calling the accelerated wrappers of the PSA_WANTed algorithms, or, if acceleration is not supported, by calling the Mbed TLS 3.x software implementation. For enabling only accelerated functionality, see the next list item.

  • Enable all the MBEDTLS_PSA_ACCEL macros in this config file that are accelerated and are required for your project. The names for these generally mirror the PSA_WANT macros. They let the build system know whether or not to include the software implementation. So, generally, the more MBEDTLS_PSA_ACCEL macros are enabled, the smaller the binary size, as less software is compiled in.

  • Please refer to the driver-only-builds.md documentation file for enablement of specific algorithms.

Example#

For example, if you PSA_WANT AES CMAC, you must PSA_WANT the AES key type, as well as CMAC. This means that PSA_WANT_KEY_TYPE_AES and PSA_WANT_ALG_CMAC need to be enabled.

If there is CMAC acceleration via PSA implemented on your device, you can enable MBEDTLS_PSA_ACCEL_ALG_CMAC to prevent the inclusion of Mbed TLS 3.x software implementation of CMAC in the build.