Hardware requirements#
Micro USB cable
MIMXRT700-EVK board
Personal Computer
RK055AHD091 MIPI panel (Not necessary if use other panel)
RK055MHD091 MIPI panel (Not necessary if use other panel)
OV7670 module Board settings ============ To use MIPI panel: Connect MIPI panel to J52.
Prepare the Demo#
The demo use MIPI RK055MHD091 panel by default, to use MIPI RK055AHD091 panel, change the macro DEMO_PANEL to 0 in mcux_config.h.
Connect a micro USB cable between the PC host and the USB port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo CM33#
When the demo runs successfully, you will find the video is dislayed on the
panel of RK055AHD091 or RK055MHD091.
and the terminal will display the following:
EZH-V flexIO DVP example started
Frame Update Rate: 28 fps
Frame Update Rate: 28 fps
Note:#
Connect the OV7670 camera sensor to J53 connector short 2-3 for JP7
Note:#
If the camera frame buffer is placed in SRAM P18~P29, and camera resolution is set to 640x480, the EZHV firmware doesn’t work at 30Hz frame rate, 15Hz frame rate works. Root cause is accessing to these RAM_ARBITER1 partitions needs more clock cycles, so the EZHV can’t write camera data to the buffers in time.