Hardware requirements#
Micro USB cable
MIMXRT700-EVK
Personal Computer
TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika. (Named as SSD1963 panel in project. Not necessary if use MIPI panel)
LCD_PAR_S035 (Not necessary if use MIPI panel)
RK055AHD091 MIPI panel (Not necessary if use other panel)
RK055MHD091 MIPI panel (Not necessary if use other panel)
RaspberryPi Panel (Not necessary if use other panel)
G1120B0MIPI(RM67162) MIPI Circular Display (Not necessary if use other panel)
Board settings#
To use SSD1963 panel: Connect SSD1963 panel to J4.
To use MIPI panel: Connect MIPI panel to J52. Note ZC143AC72MIPI(CO5300) cannot be used in this example since PNG decoder can only output frames of ABGR pixel format which cannot be supported by this panel.
To use Raspberry panel: Connect the panel to J8. Then connect the panel’s 5V pin to JP43-1, GND pin to JP43-2.
Prepare the Demo#
The demo use MIPI RK055MHD091 panel by default, to use other panel, set the coresponding panel DEMO_PANEL_xxx(without ‘_SUPPORT’) to y in prj.conf under board example folder before project generation. The supported panels can be found in examples_boards<board>\project_segments\display_support\Kconfig.prjseg. Or change the macro DEMO_PANEL in mcux_config.h of the project, which number represents which panel can be found in display_support.h and mcux_config.h
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J54) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs, the screen shows what described in overview.