MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MIMXRT700-EVK

  • Personal Computer

  • RK055AHD091 MIPI panel (Not necessary if use other panel. Not used in lcdif_dbi_rgb565 project)

  • RK055MHD091 MIPI panel (Not necessary if use other panel. Not used in lcdif_dbi_rgb565 project)

  • TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika. (Named as SSD1963 panel in project. Not necessary if use MIPI panel. Only used in lcdif_dbi_rgb565 project)

  • RM67162 smart MIPI panel (Not necessary if use other panel. Only used in lcdif_dbi_rgb565 project)

  • RaspberryPi Panel (Not necessary if use other panel. Not used in lcdif_dbi_rgb565 project)

  • CO5300 smart MIPI Panel (Not necessary if use other panel. Only used in lcdif_dbi_rgb565 project)

Board settings#

To use MIPI panel: Connect MIPI panel to J52.

To use RaspberryPi panel: Connect the panel to J8. Then connect the panel’s 5V pin to JP43-1, GND pin to JP43-2. Make sure the R75, R76, R79, R80 are connected.

To use SSD1963 panel: Connect SSD1963 panel to J4. Make sure to connect JP7 2&3 to use 3.3v interface.

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J54) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Build the project, to specify which panel to use, change the macro USE_DBI_PANEL(only example lcdif_dbi_rgb565) or USE_MIPI_PANEL(except example lcdif_dbi_rgb565) in lcdif_support.h

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the example runs, the screen shows what described in overview.