MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

  • RK055AHD091 panel or RK055MHD091 panel

Board settings#

Connect the MIPI panel to MIMXRT700-EVK board J105. For single_stream_repeat and context_switch examples, make sure JP65 1-2 are connected, and insert the SD card which has the pictures unziped in root folder in slot J47.

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J54) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Build the project, this project uses RK055MHD091 panel by default, to use use other panel, change the macro DEMO_PANEL in mcux_config.h. Which number represents which panel can be found in display_support.h and mcux_config.h.

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the example runs, the screen shows what described in overview.