MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MCX-N9XX-EVK board

  • Personal Computer

  • 3.5” TFT LCD module by NXP (P/N PAR-LCD-S035)

Board settings#

Attach the LCD shield to the EVK board.

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board

  2. Build the project.

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo#

If this example runs correctly, the sample GUI is displayed.

Note#

NOTE: Revision A0 chip can’t use SmartDMA for FlexIO display. Use the function Chip_GetVersion to check silicon revision. For A0 chip, BOARD_USE_FLEXIO_SMARTDMA must be set to 0, for A1 chip, BOARD_USE_FLEXIO_SMARTDMA can be set to 1 for better performance.