Hardware requirements#
Micro USB cable
MCX-N5XX-EVK board
Personal Computer
3.5” TFT LCD module by NXP (P/N PAR-LCD-S035) Rev.A
Board settings#
Attach the LCD shield to the EVK board.
Prepare the Demo#
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Build the project.
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
If this example runs correctly, the sample GUI is displayed.
Note#
NOTE: Revision A0 chip can’t use SmartDMA for FlexIO display. Use the function
Chip_GetVersion to check silicon revision. For A0 chip, BOARD_USE_FLEXIO_SMARTDMA
must be set to 0, for A1 chip, BOARD_USE_FLEXIO_SMARTDMA can be set to 1
for better performance.