Hardware requirements#
Micro USB cable
LPCXpresso55S16 board
Personal Computer
Board settings#
Master_board(SPI7) Slave_board(SPI2)
Pin Name Board Location Pin Name Board Location
MISO J9 pin 11 MISO J12 pin 5
MOSI J9 pin 9 MOSI J12 pin 9
SCK J9 pin 13 SCK J12 pin 7
SSEL1 J9 pin 2 SSEL0 J12 pin 13
The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
SPI one board interrupt example started!
SPI transfer finished!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~