Hardware requirements#
Micro USB cable
LPCXpresso51U68 board
Personal Computer
Board settings#
Populate jumper JP3. Connect SPI5 pins to SPI3 pins:
Master - SPI5 CONNECTS TO Slave - SPI3
Pin Name Board Location Pin Name Board Location
MISO J1 pin 11 MISO J4 pin 3
MOSI J1 pin 13 MOSI J4 pin 2
SCK J2 pin 8 SCK J4 pin 4
PCS2 J1 pin 15 PCS2 J4 pin 7
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
SPI one board interrupt example started!
SPI transfer finished!