MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • IMX95LPD5-EVK board

  • 12V~20V power supply

  • Personal Computer

Board settings#

This example uses NETC ENETC2 10G port.

Prepare the Demo#

  1. Connect 12V~20V power supply to the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Program the Linux BSP to SD/eMMC. Then program flash.bin of this demo.

  5. Switch SW4 to power on the board.

Note: the flash.bin is flash_all target with mx95netc.cfg System Manager image. For A core Linux BSP side usage, refer to Linux BSP User Guide “11.6.1 i.MX95 ENETC share use case”.

Running the demo#

When the demo runs, the log would be seen on the terminal like below. Both A core Linux BSP and M core share NETC ENETC2 10G port to use.

Initializing PHY...
[LINK STATE] netif=0, state=up, speed=1000M_full

************************************************
 DHCP example
************************************************
 DHCP state       : SELECTING
 DHCP state       : REQUESTING
 DHCP state       : CHECKING
 DHCP state       : BOUND

 IPv4 Address     : 192.168.0.4
 IPv4 Subnet mask : 255.255.255.0
 IPv4 Gateway     : 192.168.0.1