Hardware requirements#
Mini USB cable
FRDM-MCXC242 board
Personal Computer
Board settings#
SPI one board:
Transfer data from instance0 to instance 1 of SPI interface, SPI0 pins are connected with SPI1 pins of board
INSTANCE0 CONNECTS TO INSTANCE1
Pin Name Board Location Pin Name Board Location
MOSI J2 pin 8 MOSI J2 pin 18
MISO J2 pin 10 MISO J2 pin 20
SCK J2 pin 12 SCK J1 pin 11
PCS0 J2 pin 6 PCS0 J1 pin 9
Prepare the Demo#
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
SPI one board interrupt example started!
SPI transfer finished!