Hardware requirements#
Mini/micro USB cable
FRDM-K22F board
Personal Computer
Board settings#
No special is needed.
Prepare the Demo#
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Connect the analog signal source’s output to the input of used-defined comparator’s channel (defined as “DEMO_CMP_USER_CHANNEL” in source code.)
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
CMP interrupt Example
Then change CMP analog input, and watch the change of LED. - CMP0_IN0 (Jump J1-16) connected to VCC=3.3V(Jump J25-4): LED GREEN on - CMP0_IN0 (Jump J1-16) connected to GND(Jump J2-14): LED GREEN off