Hardware requirements#
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
RK055AHD091 panel or RK055MHD091 panel
Board settings#
Connect the MIPI panel to EVK-MIMXRT595 board J44.
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build the project, this project uses RK055MHD091 panel by default, to use the RK055AHD091 panel, change #define USE_MIPI_PANEL MIPI_PANEL_RK055MHD091 to #define USE_MIPI_PANEL MIPI_PANEL_RK055AHD091 in lcdif_support.h.
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs, the screen shows what described in overview.