MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows the output of the clockout demo in the terminal window:

Clock Output Driver Example.
Please choose one output clock.
	A -- OSC_CLK Clock.
	B -- Low Power Oscillator Clock.
	C -- FRO_DIV2 Clock.
	D -- Main Clock.
	E -- Dsp Main Clock.
	F -- Main System PLL.
	G -- SYSPLL0 AUX0_PLL_Clock.
	H -- DSP PLL Clock.
	I -- SYSPLL0 AUX1_PLL_Clock.
	J -- AUDIO PLL Clock.
	K -- 32 KHz RTC Clock.

To measure the output clock signal, please use the oscilloscope to probe JP27_2.