MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MIMX8ULP-EVK/EVK9 board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

  • Microphone

Board settings#

Connect microphone module to EVK board: 3V->J20-8 GND->J20-7 CLK->J21-4 DATA->J21-3

Please note this application can’t support running with Linux BSP!

Prepare the Demo#

  1. Connect 5V power supply and JLink Plus to the board, switch SW10 to power on the board

  2. Connect a micro USB cable between the host PC and the J17 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, you can hear the sound gathered from microphone and the log would be seen on the OpenSDA terminal like:

Audio demo started. Initialize pins and codec on core 'Cortex-M33'
Pins and codec initialized.
DSP starts on core 'fusion_nxp02_dsp_prod'
MIC->DMA->I2S->CODEC running