Examples#
The table below lists the example applications provided.
Application |
Device type |
|---|---|
Coordinator |
Coordinator/Trust center |
Router |
Router |
End Device RX On |
End Device (Non-sleeping) |
End Device RX Off when Idle |
End Device (Sleeping) |
The examples are provided as part of the wireless examples for ZigBee. The binaries generated by these examples are targeted to run on the FRDM-MCXW71 board, FRDM-MCXW72, MCX-W71-EVK, MCX-W72-EVK, RD-RW612-BGA, and FRDM-RW612 boards.
Note: The RW612 platform does not support the RX OFF Application use case currently.
FRDM-MCXW7x board#
The FRDM-MCXW7x board is used for the ZigBee examples described in this document. The important LEDs and user control buttons are highlighted, as shown in the figure, FRDM-MCXW7x board below.
Parent topic:Examples
FRDM-MCXW71 / FRDM-MCXW72 board#
The FRDM-MCXW71 or the FRDM-MCXW72 board can be used for the ZigBee examples described in this document. The important LEDs and user control buttons are highlighted, as shown in the figure below.
Parent topic:Examples
RD-RW612-BGA board#
The FRDM-RW612 board can be used for the ZigBee examples described in this document. The important LEDs and user control buttons are highlighted, as shown in the figure, RD-RW612-BGA board below.

Parent topic:Examples
FRDM-RW612 board#
The FRDM-RW612 board is used for the ZigBee examples described in this document. The important LEDs and user control buttons are highlighted, as shown in the figure, FRDM-RW612 board below.

Parent topic:Examples
MCX-W71-EVK / MCX-W72-EVK board#
The MCX-W71-EVK or the MCX-W72-EVK board can be used for the ZigBee examples described in this document. The board is shown in the figure below.

Parent topic:Examples