tsZLL_CommissionEndpointClusterInstances#
This structure holds information about the Touchlink Commissioning cluster instance on an endpoint.
typedef struct PACK
{
#if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_SERVER)
tsZCL_ClusterInstance sZllCommissionServer;
#endif
#if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_CLIENT)
tsZCL_ClusterInstance sZllCommissionClient;
#endif
} tsZLL_CommissionEndpointClusterInstances;
where:
s``ZllCommissionServeris a ZCL structure containing information about the Touchlink Commissioning cluster server instance (refer to Section 6.1.16).s``ZllCommissionClientis a ZCL structure containing information about the Touchlink Commissioning cluster client instance (refer to Section 6.1.16).
Parent topic:Structures