MCUXpresso SDK Documentation

tsCLD_ZllCommission_IdentifyReqCommandPayload

tsCLD_ZllCommission_IdentifyReqCommandPayload#

This structure is used to hold the payload data for a Touchlink Identify Request command.

typedef struct
{
    uint32  u32TransactionId;
    uint16  u16Duration;
} tsCLD_ZllCommission_IdentifyReqCommandPayload;

where:

  • u32TransactionId is the 32-bit Inter-PAN Transaction Identifier of the request. This is a random number generated and inserted automatically.

  • u16Duration specifies the length of time (in seconds) that the target node is to remain in identify mode. The possible values are:

    • 0x0000: Exit identify mode immediately

    • 0x0001–0xFFFE: Number of seconds to remain in identify mode

    • 0xFFFF: Remain in identify mode for the default time for the target node

      • If the target node is unable to provide accurate timings, it will attempt to remain in identify mode for as close to the requested time as possible

Parent topic:Structures