MCUXpresso SDK Documentation

eCLD_ZllCommissionCommandScanRspCommandSend

eCLD_ZllCommissionCommandScanRspCommandSend#

PUBLIC teZCL_Status eCLD_ZllCommissionCommandScanRspCommandSend(
    ZPS_tsInterPanAddress *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ZllCommission_ScanRspCommandPayload
*psPayload);

Description#

This function is used to send a Scan Response command containing information about the local node in reply to a received Scan Request from a remote node. The command is sent as an inter-PAN message.

A pointer must be provided to a structure containing the data to be returned.

The specified Transaction Sequence Number (TSN) of the response must match the TSN of the corresponding request, as this will allow the response to be paired with the request at the destination.

Parameters#

  • psDestinationAddress                Pointer to stucture containing PAN ID and address information for target node

  • pu8TransactionSequenceNumber        Pointer to location containing the Transaction Sequence Number (TSN) of the response

  • psPayload        Pointer to structure containing payload data for the Scan Response command (see Section 44.8.6)

Returns#

  • E_ZCL_SUCCESS

Parent topic:Touchlink functions