MCUXpresso SDK Documentation

eCLD_ZllCommissionCommandNetworkJoinEndDeviceRspCommandSend

eCLD_ZllCommissionCommandNetworkJoinEndDeviceRspCommandSend#

PUBLIC teZCL_Status eCLD_ZllCommissionCommandNetworkJoinEndDeviceRspCommandSend(
ZPS_tsInterPanAddress *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_ZllCommission_NetworkJoinEndDeviceRspCommandPayload
*psPayload);

Description#

This function is used to send a Network Join End Device Response command to confirm that the local (End Device) node is ready to join a network in reply to a received Network Join End Device Request from a remote node. The command is sent as an inter-PAN message.

A pointer must be provided to a structure containing the data to be returned.

The specified Transaction Sequence Number (TSN) of the response must match the TSN of the corresponding request, as this will allow the response to be paired with the request at the destination.

Parameters#

  • psDestinationAddress Pointer to stucture containing PAN ID and address information for target node

  • pu8TransactionSequenceNumber Pointer to location containing the Transaction Sequence Number (TSN) of the response

  • psPayload Pointer to structure containing payload data for the Network Join End Device Response command (see Section 44.8.16)

Returns#

  • E_ZCL_SUCCESS

Parent topic:Touchlink functions