MCUXpresso SDK Documentation

Structures#

Custom Data Structure#

The Thermostat cluster requires extra storage space to be allocated for use by internal functions. The structure definition for this storage is shown below:

typedef struct
{
    tsZCL_ReceiveEventAddress         sReceiveEventAddress;
    tsZCL_CallBackEvent               sCustomCallBackEvent;
    tsCLD_ThermostatCallBackMessage   sCallBackMessage;
} tsCLD_ThermostatCustomDataStructure;

The fields are for internal use and no knowledge of them is required.

Parent topic:Structures

tsCLD_ThermostatCallBackMessage#

For a Thermostat cluster event, the eEventType field of the tsZCL_CallBackEvent structure is set to E_ZCL_CBET_CLUSTER_CUSTOM. This event structure also contains an element sClusterCustomMessage, which is itself a structure containing a field pvCustomData. This field is a pointer to the following tsCLD_ThermostatCallBackMessage structure:

typedef struct
{
    uint8                                           u8CommandId;
    union
    {
      tsCLD_Thermostat_SetpointRaiseOrLowerPayload *psSetpointRaiseOrLowerPayload;
    } uMessage;
} tsCLD_ThermostatCallBackMessage; 

where:

  • u``8CommandId indicates the type of Thermostat cluster command that has been received - there is only one possibility: E_CLD_THERMOSTAT_CMD_SETPOINT_RAISE_LOWER

  • u``Message is a union containing the command payload in the following form: psSetpointRaiseOrLowerPayload is a pointer to a structure containing the payload of a ‘Setpoint Raise Or Lower’ command - see Section 33.9.3.

Parent topic:Structures

tsCLD_Thermostat_SetpointRaiseOrLowerPayload#

This stucture contains the payload of a ‘Setpoint Raise Or Lower’ command (from the cluster client) which requests a change the value of the attribute i16OccupiedHeatingSetpoint and/or the attribute i16OccupiedCoolingSetpoint.

typedef struct
{
    zenum8                 eMode;
    zint8                  i8Amount;
}tsCLD_Thermostat_SetpointRaiseOrLowerPayload;

where:

  • eMode indicates the Thermostat operating mode to which the command relates, one of:

    • E_CLD_THERMOSTAT_SRLM_HEAT (Heating)

    • E_CLD_THERMOSTAT_SRLM_COOL (Cooling)

    • E_CLD_THERMOSTAT_SRLM_BOTH (Heating and Cooling)

  • i8Amount represents the value (in two’s complement form) by which the setpoint corresponding to the specified operating mode is to be changed

Parent topic:Structures

Parent topic:Thermostat Cluster