MCUXpresso SDK Documentation

tsZCL_CommandDiscoveryIndividualResponse

tsZCL_CommandDiscoveryIndividualResponse#

This structure contains information about an individual command reported in a Command Discovery response (see Section 2.9).

typedef struct
{
    uint8  u8CommandEnum;
    uint8  u8CommandIndex;
} tsZCL_CommandDiscoveryIndividualResponse;

where:

  • u8CommandEnum is the Command ID of the reported command

  • u8CommandIndex is the index of the reported command in the response payload

The above structure is contained in the tsZCL_CallBackEvent event structure, detailed in Section 6.2, when the field eEventType is set to E_ZCL_CBET_DISCOVER_INDIVIDUAL_COMMAND_RECEIVED_RESPONSE or E_ZCL_CBET_DISCOVER_INDIVIDUAL_COMMAND_GENERATED_RESPONSE.

Parent topic:General Structures