tsZCL_AttributeDiscoveryExtendedResponse
This structure contains details of an attribute reported in a ‘discover attributes extended’ response. It is contained in a ZCL event of type E_ZCL_CBET_DISCOVER_INDIVIDUAL_ATTRIBUTE_EXTENDED_RESPONSE.
typedef struct
{
bool_t bDiscoveryComplete;
uint16 u16AttributeEnum;
teZCL_ZCLAttributeType eAttributeDataType;
uint8 u8AttributeFlags;
}tsZCL_AttributeDiscoveryExtendedResponse;
where:
bDiscoveryCompleteindicates whether this is the final attribute from a ‘discover attributes’ to be reported:TRUE - final attribute
FALSE - not final attribute
u16AttributeEnumis the identifier of the attribute being reportedeAttributeDataTypeindicates the data type of the attribute being reported (see Section 7.1.3)u8AttributeFlagsis a 5-bit bitmap indicating the accessibility of the reported attribute (for details of the access types, refer to Section 2.3.1) - a bit is set to ‘1’ if the corresponding access type is supported, as follows:
Bit |
Access Type |
|---|---|
0 |
Read |
1 |
Write |
2 |
Reportable |
3 |
Scene |
4 |
Global |
5-7 |
Reserved |
The above structure is contained in the tsZCL_CallBackEvent event structure, detailed in Section 6.2, when the field eEventType is set to E_ZCL_CBET_DISCOVER_INDIVIDUAL_ATTRIBUTE_EXTENDED_RESPONSE.
Parent topic:General Structures