Event Structure
The tsZCL_CallBackEvent structure, in which an event is wrapped, is as follows:
typedef struct
{
teZCL_CallBackEventType eEventType;
uint8 u8TransactionSequenceNumber;
uint8 u8EndPoint;
teZCL_Status eZCL_Status;
union {
tsZCL_IndividualAttributesResponse sIndividualAttributeResponse;
tsZCL_DefaultResponse sDefaultResponse;
tsZCL_TimerMessage sTimerMessage;
tsZCL_ClusterCustomMessage sClusterCustomMessage;
tsZCL_AttributeReportingConfigurationRecord
sAttributeReportingConfigurationRecord;
tsZCL_AttributeReportingConfigurationResponse
sAttributeReportingConfigurationResponse;
tsZCL_AttributeDiscoveryResponse sAttributeDiscoveryResponse;
ZCL_AttributeStatusRecord sReportingConfigurationResponse;
tsZCL_ReportAttributeMirror sReportAttributeMirror;
uint32 u32TimerPeriodMs;
tsZCL_CommandDiscoveryIndividualResponse
sCommandsReceivedDiscoveryIndividualResponse;
tsZCL_CommandDiscoveryResponse sCommandsReceivedDiscoveryResponse;
tsZCL_CommandDiscoveryIndividualResponse
sCommandsGeneratedDiscoveryIndividualResponse;
tsZCL_CommandDiscoveryResponse sCommandsGeneratedDiscoveryResponse;
tsZCL_AttributeDiscoveryExtendedResponse
sAttributeDiscoveryExtenedResponse;
}uMessage ;
ZPS_tsAfEvent *pZPSevent;
tsZCL_ClusterInstance *psClusterInstance;
} tsZCL_CallBackEvent;
The fields of this structure are fully described Section 6.2.
In the tsZCL_CallBackEvent structure, the eEventType field defines the type of event being posted - the various event types are described in Section 3.3 below. The union and remaining fields are each relevant to only specific event types.
Parent topic:Event Handling