Structures
Custom Data Structure
The Scenes cluster requires extra storage space to be allocated to be used by internal functions. The structure definition for this storage is shown below:
typedef struct
{
DLIST lScenesAllocList;
DLIST lScenesDeAllocList;
tsZCL_ReceiveEventAddress sReceiveEventAddress;
tsZCL_CallBackEvent sCustomCallBackEvent;
tsCLD_ScenesCallBackMessage sCallBackMessage;
tsCLD_ScenesTableEntry
asScenesTableEntry[CLD_SCENES_MAX_NUMBER_OF_SCENES];
} tsCLD_ScenesCustomDataStructure;
The fields are for internal use and no knowledge of them is required.
Parent topic:Structures
Custom Command Payloads
The following structures contain the payloads for the Scenes cluster custom commands.
Add Scene Request Payload
typedef struct
{
uint16 u16GroupId;
uint8 u8SceneId;
uint16 u16TransitionTime;
tsZCL_CharacterString sSceneName;
tsCLD_ScenesExtensionField sExtensionField;
} tsCLD_ScenesAddSceneRequestPayload;
where:
u16GroupIdis the group ID with which the scene is associated (0x0000 if there is no association with a group)u8SceneIdis the ID of the scene to be added to the Scene table (the Scene ID must be unique within the group associated with the scene)u16TransitionTimeis the amount of time, in seconds, that the device takes to switch to this scenesSceneNameis an optional character string (of up to 16 characters) representing the name of the scenesExtensionFieldis a structure containing the attribute values of the clusters to which the scene relates
View Scene Request Payload
typedef struct
{
uint16 u16GroupId;
uint8 u8SceneId;
} tsCLD_ScenesViewSceneRequestPayload;
where:
u16GroupIdis the group ID with which the desired scene is associatedu8SceneIdis the scene ID of the scene to be viewed
Remove Scene Request Payload
typedef struct
{
uint16 u16GroupId;
uint8 u8SceneId;
} tsCLD_ScenesRemoveSceneRequestPayload;
where:
u16GroupIdis the group ID with which the relevant scene is associatedu8SceneIdis the scene ID of the scene to be deleted from the Scene table
Remove All Scenes Request Payload
typedef struct
{
uint16 u16GroupId;
} tsCLD_ScenesRemoveAllScenesRequestPayload;
where u16GroupId is the group ID for which all scenes are to be deleted.
Store Scene Request Payload
typedef struct
{
uint16 u16GroupId;
uint8 u8SceneId;
} tsCLD_ScenesStoreSceneRequestPayload;
where:
u16GroupIdis the group ID with which the relevant scene is associatedu8SceneIdis the scene ID of the scene in which the captured cluster settings are to be stored
Recall Scene Request Payload
typedef struct
{
uint16 u16GroupId;
uint8 u8SceneId;
} tsCLD_ScenesRecallSceneRequestPayload;
where:
u16GroupIdis the group ID with which the relevant scene is associatedu8SceneIdis the scene ID of the scene from which cluster settings are to be retrieved and applied
Get Scene Membership Request Payload
typedef struct
{
uint16 u16GroupId;
} tsCLD_ScenesGetSceneMembershipRequestPayload;
where u16GroupId is the group ID for which associated scenes are required.
Enhanced Add Scene Request Payload
typedef struct
{
uint16 u16GroupId;
uint8 u8SceneId;
uint16 u16TransitionTime100ms;
tsZCL_CharacterString sSceneName;
tsCLD_ScenesExtensionField sExtensionField;
} tsCLD_ScenesEnhancedAddSceneRequestPayload;
where:
u16GroupIdis the group ID with which the scene is associated (0x0000 if there is no association with a group)u8SceneIdis the ID of the scene to be added to the Scene table (the Scene ID must be unique within the group associated with the scene)u16TransitionTime100msis the amount of time, in tenths of a second, that the device takes to switch to this scenesSceneNameis an optional character string (of up to 16 characters) representing the name of the scenesExtensionFieldis a structure containing the attribute values of the clusters to which the scene relates
View Scene Request Payload
typedef struct
{
uint16 u16GroupId;
uint8 u8SceneId;
} tsCLD_ScenesEnhancedViewSceneRequestPayload;
where:
u16GroupIdis the group ID with which the desired scene is associatedu8SceneIdis the scene ID of the scene to be viewed
Copy Scene Request Payload
typedef struct
{
uint8 u8Mode;
uint16 u16FromGroupId;
uint8 u8FromSceneId;
uint16 u16ToGroupId;
uint8 u8ToSceneId;
} tsCLD_ScenesCopySceneRequestPayload;
where:
u8Modeis a bitmap indicating the required copying mode (only bit 0 is used):If bit 0 is set to ‘1’, then ‘copy all scenes’ mode is used, in which all scenes associated with the source group are duplicated for the destination group (and the scene ID fields are ignored)
If bit 0 is set to ‘0’, then a single scene is copied
u16FromGroupIdis the source group IDu8FromSceneIdis the source scene ID (ignored for ‘copy all scenes’ mode)u16ToGroupIdis the destination group IDu8ToSceneIdis the destination scene ID (ignored for ‘copy all scenes’ mode)
Parent topic:Structures
Custom Command Responses
The Scenes cluster generates responses to certain custom commands. The responses which contain payloads are detailed below:
Add Scene Response Payload
typedef struct
{
zenum8 eStatus;
uint16 u16GroupId;
uint8 u8SceneId;
} tsCLD_ScenesAddSceneResponsePayload;
where:
eStatusis the outcome of the Add Scene command (success or invalid)u16GroupIdis the group ID with which the added scene is associatedu8SceneIdis the scene ID of the added scene
View Scene Response Payload
typedef struct
{
zenum8 eStatus;
uint16 u16GroupId;
uint8 u8SceneId;
uint16 u16TransitionTime;
tsZCL_CharacterString sSceneName;
tsCLD_ScenesExtensionField sExtensionField;
} tsCLD_ScenesViewSceneResponsePayload;
where:
eStatusis the outcome of the View Scene command (success or invalid)u16GroupIdis the group ID with which the viewed scene is associatedu8SceneIdis the scene ID of the viewed sceneu16TransitionTimeis the amount of time, in seconds, that the device takes to switch to the viewed scenesSceneNameis an optional character string (of up to 16 characters) representing the name of the viewed scenesExtensionFieldis a structure containing the attribute values of the clusters to which the viewed scene relates
Remove Scene Response Payload
typedef struct
{
zenum8 eStatus;
uint16 u16GroupId;
uint8 u8SceneId;
} tsCLD_ScenesRemoveSceneResponsePayload;
where:
eStatusis the outcome of the Remove Scene command (success or invalid)u16GroupIdis the group ID with which the removed scene is associatedu8SceneIdis the scene ID of the removed scene
Remove All Scenes Response Payload
typedef struct
{
zenum8 eStatus;
uint16 u16GroupId;
} tsCLD_ScenesRemoveAllScenesResponsePayload;
where:
eStatusis the outcome of the Remove All Scenes command (success or invalid)u16GroupIdis the group ID with which the removed scenes are associated
Store Scene Response Payload
typedef struct
{
zenum8 eStatus;
uint16 u16GroupId;
uint8 u8SceneId;
} tsCLD_ScenesStoreSceneResponsePayload;
where:
eStatusis the outcome of the Store Scene command (success or invalid)u16GroupIdis the group ID with which the stored scene is associatedu8SceneIdis the scene ID of the stored scene
Get Scene Membership Response Payload
typedef struct
{
zenum8 eStatus;
uint8 u8Capacity;
uint16 u16GroupId;
uint8 u8SceneCount;
uint8 *pu8SceneList;
} tsCLD_ScenesGetSceneMembershipResponsePayload;
where:
eStatusis the outcome of the Get Scene Membership command (success or invalid)u8Capacityis the capacity of the Scene table of the device to receive more scenes - that is, the number of scenes that may be added (special values: 0xFE means that at least one more scene may be added, a higher value means that the remaining capacity of the table is unknown)u16GroupIdis the group ID to which the query relatesu8SceneCountis the number of scenes in the list of the next fieldpu8SceneListis a pointer to the returned list of scenes from those queried that exist on the device, where each scene is represented by its scene ID
Enhanced Add Scene Response Payload
typedef struct
{
zenum8 eStatus;
uint16 u16GroupId;
uint8 u8SceneId;
} tsCLD_ScenesEnhancedAddSceneResponsePayload;
where:
eStatusis the outcome of the Enhanced Add Scene command (success or invalid)u16GroupIdis the group ID with which the added scene is associatedu8SceneIdis the scene ID of the added scene
Enhanced View Scene Response Payload
typedef struct
{
zenum8 eStatus;
uint16 u16GroupId;
uint8 u8SceneId;
uint16 u16TransitionTime;
tsZCL_CharacterString sSceneName;
tsCLD_ScenesExtensionField sExtensionField;
} tsCLD_ScenesEnhancedViewSceneResponsePayload;
where:
eStatusis the outcome of the Enhanced View Scene command (success or invalid)u16GroupIdis the group ID with which the viewed scene is associatedu8SceneIdis the scene ID of the viewed sceneu16TransitionTimeis the amount of time, in seconds, that the device takes to switch to the viewed scenesSceneNameis an optional character string (of up to 16 characters) representing the name of the viewed scenesExtensionFieldis a structure containing the attribute values of the clusters to which the viewed scene relates
Copy Scene Response Payload
typedef struct
{
uint8 u8Status;
uint16 u16FromGroupId;
uint8 u8FromSceneId;
} tsCLD_ScenesCopySceneResponsePayload;
where:
u8Statusis the outcome of the Copy Scene command (success, invalid scene, or insufficient space for new scene)u16FromGroupIdis the source group ID for the copyu8FromSceneIdis the source scene ID for the copy
Parent topic:Structures
Scenes Table Entry
The following structure contains the data for a Scenes table entry (containing a saved scene):
typedef struct
{
DNODE dllScenesNode;
bool bActive;
bool bInTransit;
uint16 u16GroupId;
uint8 u8SceneId;
uint16 u16TransitionTime;
uint32 u32TransitionTimer;
uint8 u8SceneNameLength;
uint8 au8SceneName[CLD_SCENES_MAX_SCENE_NAME_LENGTH + 1];
uint16 u16SceneDataLength;
uint8 au8SceneData[CLD_SCENES_MAX_SCENE_STORAGE_BYTES];
#ifdef CLD_SCENES_TABLE_SUPPORT_TRANSITION_TIME_IN_MS
uint8 u8TransitionTime100ms;
#endif
} tsCLD_ScenesTableEntry;
where:
bActiveis a boolean value indicating whether the scene is active (TRUE) or inactive (FALSE).bInTransitis a boolean value indicating whether the scene is in a transitional state (TRUE) or a constant active/inactive state (FALSE).u16GroupIdis the identifier of the group to which the scene applies (the value 0x0000 is used to indicate that the scene is not associated with a group).u8SceneIdis the identifier of the scene and must be a unique value within the group with which the scene is associated.u16TransitionTimeis the length of time, in seconds, that the device takes to move from its current state to the scene state.u32TransitionTimeris the elapsed time, in milliseconds, since the start of a currently active transition to the scene.u8SceneNameLengthis the number of characters in the name of the scene (and therefore the size of the arrayau8SceneName[]below). The value must not be greater than CLD_SCENES_MAX_SCENE_NAME_LENGTH, which is set in the compile-time options (see Section 13.9).au8SceneName[]is an array containing the name of the scene, with one ASCII character in each array element. The number of elements in the array must be set inu8SceneNameLengthabove.u16SceneDataLengthis the number of items of data for the scene (and therefore the size of the arrayau8SceneData[]below). The value must not be greater than CLD_SCENES_MAX_SCENE_STORAGE_BYTES, which is set in the compile-time options (see Section 13.9).au8SceneData[]is an array containing the data for the scene, with one data item in each array element. The data stored is dependent on the cluster to which the scene data applies. The number of elements in the array must be set inu16SceneDataLengthabove.u8TransitionTime100 ms is an optional that allows a fractional part to be added to the transition time (u16TransitionTime) of the scene. This value represents the number of tenths of a second in the range 0x00 to 0x09.
Parent topic:Structures
Parent topic:Scenes Cluster