eCLD_ScenesStore#
teZCL_Status eCLD_ScenesStore(
uint8 u8SourceEndPointId,
uint16 u16GroupId,
uint8 u8SceneId);
Description#
This function adds a new scene on the specified local endpoint, based on the current cluster attribute values of the device- that is, saves the current attribute values of the device to a new entry of the Scenes table on the endpoint. The group ID associated with the scene must also be specified (or set to 0x0000 if there is no associated group).
If a scene with the specified scene ID and group ID exists in the table, the existing entry is overwritten. The previous scene data in this entry is lost, except for the transition time field and the scene name field - these fields are left unchanged.
Parameters#
u8SourceEndPointId: Number of local endpoint on which Scene table entry is to be added.
*u16GroupId:*16-bit group ID/address of associated group (or 0x0000 if no group)
u8SceneId: 8-bit scene ID of scene
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
Parent topic:Functions