tsSE_PricePublishConversionCmdPayload#
This structure is used to hold information to be added to a conversion factor list of a Price cluster:
typedef struct {
uint32 u32IssuerEventId;
uint32 u32StartTime;
uint32 u32ConversionFactor;
zbmap8 u8ConversionFactorTrailingDigit;
}tsSE_PricePublishConversionCmdPayload;
where:
u32IssuerEventIdis a unique identifier for the conversion factor information - the higher the value, the more recently the information was issuedu32StartTimeis the start-time of the conversion factor value. This is the time at which the conversion factor value is scheduled to become activeu32ConversionFactoris used only for gas and accounts for the variation in the volume of gas with temperature and pressure (the value is dimensionless)u8ConversionFactorTrailingDigitis an 8-bit bitmap which indicates the location of the decimal point in theu32ConversionFactorfield. The most significant 4 bits indicate the number of digits after the decimal point. The remaining bits are reserved
Parent topic:Structures