eSE_PriceGetCalorificValueSend#
teZCL_Status eSE_PriceGetCalorificValueSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
uint32 u32StartTime,
uint8 u8NumberOfEvents);
Description#
The function can be used on a Price cluster client to send a Get Calorific Value request to the Price cluster server. Therefore, it is used by a device (such as an IPD) to obtain scheduled calorific values from the ESP. The function allows scheduled calorific values to be obtained with start-times greater than or equal to a specified time, u32StartTime.
The ESP should respond with a Publish Calorific Value command containing up to u8NumberOfEvent scheduled calorific values. The Price cluster on the receiving client processes the response by updating the local calorific value list, as follows. For each calorific value received in the response, the event E_SE_PRICE_CALORIFIC_VALUE_ADD is generated.
A pointer must be specified to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request.
Parameters#
u8SourceEndPointId: Number of the local endpoint through which the request is sent
u8DestinationEndPointId: Number of the remote endpoint to which the request is sent
psDestinationAddress: Pointer to a structure containing the address of the remote node to which the request is sent
pu8TransactionSequenceNumber: Pointer to a location to store the Transaction Sequence Number (TSN) of the request
u32StartTime: Earliest start-time of scheduled calorific values to be returned - a setting of 0 returns the value that is currently active and values with start-times in the future
u8NumberOfEvents: Maximum number of calorific values to be returned as a result of this request
Returns#
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZTRANSMIT_FAIL
Parent topic:Functions