Structures
Custom Data Structure
The On/Off cluster requires extra storage space to be allocated to be used by internal functions. The structure definition for this storage is shown below:
typedef struct
{
uint8 u8Dummy;
} tsCLD_OnOffCustomDataStructure;
The fields are for internal use and no knowledge of them required.
Parent topic:Structures
Custom Command Payloads
Off With Effect Request Payload
typedef struct
{
zuint8 u8EffectId;
zuint8 u8EffectVariant;
} tsCLD_OnOff_OffWithEffectRequestPayload;
where:
u8EffectIdindicates the required ‘off effect’:0x00 - Fade
0x01 - Rise and fall
All other values are reserved.
u8EffectVariantindicates the required variant of the specified ‘off effect’ - the interpretation of this field depends on the value ofu8EffectId, as indicated in the table below.
u8EffectId |
u8EffectVariant |
Description |
|---|---|---|
0x00 |
0x00 |
Fade to off in 0.8 seconds (default) |
0x01 |
No fade |
|
0x02 |
Reduce brightness by 50 % in 0.8 seconds then fade to off in 4 seconds |
|
0x03-0xFF |
Reserved |
|
0x01 |
0x00 |
Increase brightness by 20 % (if possible) in 0.5 seconds then fade to off in 1 second (default) |
0x01-0xFF |
Reserved |
|
0x02-0xFF |
0x00-0xFF |
Reserved |
On With Timed Off Request Payload
typedef struct
{
zuint8 u8OnOff;
zuint16 u16OnTime;
zuint16 u16OffTime;
} tsCLD_OnOff_OnWithTimedOffRequestPayload;
where:
u8OnOffindicates when the command can be accepted:0x00 - at all times (apart from in waiting time, if implemented)
0x01 - only when light is on
All other values are reserved.
u16OnTimeis the ‘on time’, expressed in tenths of a second in the range 0x0000 to 0xFFFE.u16OffTimeis the ‘off waiting time’, expressed in tenths of a second in the range 0x0000 to 0xFFFE
Parent topic:Structures
Parent topic:On/Off Cluster