eCLD_OnOffCreateOnOff
teZCL_Status eCLD_OnOffCreateOnOff(
tsZCL_ClusterInstance *psClusterInstance,
bool_t bIsServer,
tsZCL_ClusterDefinition *psClusterDefinition,
void *pvEndPointSharedStructPtr,
uint8 *pu8AttributeControlBits,
tsCLD_OnOffCustomDataStructure
*psCustomDataStructure);
Description
This function creates an instance of the On/Off cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.
The function must be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function creates an On/Off cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions.
Note: Do not call this function for an endpoint on which a standard ZigBee device is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function.
When used, this function must be the first On/Off cluster function called in the application, and must be called after the stack has been started and after the ZCL has been initialized.
The function requires an array to be declared for internal use, which contains one element (of type uint8) for each attribute of the cluster. The array length should therefore equate to the total number of attributes supported by the On/Off cluster. The function initialises the array elements to zero.
Parameters
psClusterInstance: Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initialising individual structure fields.
bIsServer: Type of cluster instance (server or client) to be created:
TRUE - server
FALSE - client
psClusterDefinition: Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the On/Off cluster. This parameter can refer to a pre-filled structure called
sCLD_OnOffwhich is provided in the OnOff.h file.pvEndPointSharedStructPtr: Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type
tsCLD_OnOffwhich defines the attributes of On/Off cluster. The function initialises the attributes with default values.pu8AttributeControlBits: Pointer to an array of uint8 values, with one element for each attribute in the cluster (see above)
psCustomDataStructure: Pointer to a structure containing the storage for internal functions of the cluster (see Section 14.8.1)
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
Parent topic:Functions