Structures
Custom Data Structure
The Identity cluster requires extra storage space to be allocated to be used by internal functions. The structure definition for this storage is shown below:
typedef struct
{
tsZCL_ReceiveEventAddress sReceiveEventAddress;
tsZCL_CallBackEvent sCustomCallBackEvent;
tsCLD_IdentifyCallBackMessage sCallBackMessage;
} tsCLD_IdentifyCustomDataStructure;
The fields are for internal use and no knowledge of them is required.
Parent topic:Structures
Custom Command Payloads
The following structure contains the payload for an Identify cluster custom command (sent using the function eCLD_IdentifyCommandIdentifyRequestSend()):
/* Identify request command payload */
typedef struct
{
zuint16 u16IdentifyTime;
} tsCLD_Identify_IdentifyRequestPayload;
where u16IdentifyTime is the amount of time, in seconds, for which the target device is to remain in identification mode. If this element is set to 0x0000 and the target device is in identification mode, the mode is terminated immediately.
Parent topic:Structures
Custom Command Responses
The following structure contains the response to a query whether a device is in identification mode (the original query is sent using the function eCLD_IdentifyCommandIdentifyQueryRequestSend()):
/* Identify query response command payload */
typedef struct
{
zuint16 u16Timeout;
} tsCLD_Identify_IdentifyQueryResponsePayload;
where u16Timeout is the amount of time, in seconds, that the responding device remains in identification mode.
Parent topic:Structures
EZ-mode Commissioning Command Payloads
The structures described below may be used when the Identify cluster is used with EZ-mode commissioning (which is part of the ZigBee Base Device functionality and is described in the ZigBee Devices User Guide (JNUG3131)).
‘EZ-Mode Invoke’ Command Payload
The following structure is used when sending an ‘EZ-mode Invoke’ command (using the eCLD_IdentifyEZModeInvokeCommandSend() function).
typedef struct
{
zbmap8 u8Action;
} tsCLD_Identify_EZModeInvokePayload;
where u8Action is a bitmap specifying the EZ-mode commissioning actions to be performed on the destination device - a bit is set to ‘1’ if the corresponding action is required, or to ‘0’ if it is not required:
Bits |
Action |
|---|---|
0 |
Factory Reset - clears all bindings, group table entries, and the |
1 |
Network Steering - puts the device into the ‘Network Steering’ phase |
2 |
Find and Bind - puts the device into the ‘Find and Bind’ phase |
3 - 7 |
Reserved |
‘Update Commission State’ Command Payload
The following structure is used when sending an ‘Update Commission State’ command (using the eCLD_IdentifyUpdateCommissionStateCommandSend() function), which requests an update to the value of the u8CommissionState attribute (for the definition of the attribute, refer to Section 11.2).
typedef struct
{
zenum8 u8Action;
zbmap8 u8CommissionStateMask;
} tsCLD_Identify_UpdateCommissionStatePayload;
where:
u8Actionis a value specifying the action to perform (set or clear) on theu8CommissionStatebits specified throughu8CommissionStateMask:1: Set the specified bits to ‘1’.
2: Clear the specified bits to ‘0’.
All other values are reserved.
u8CommissionStateMaskis a bitmap in which the bits correspond to the bits of theu8CommissionStateattribute. A bit of this field indicates whether the corresponding attribute bit is to be updated (according to the action specified inu8Action):If a bit is set to ‘1’, the corresponding
u8CommissionStatebit should be updated.If a bit is set to ‘0’, the corresponding
u8CommissionStatebit should not be updated.
Parent topic:Structures
Parent topic:Identify Cluster