eCLD_IdentifyCreateIdentify
teZCL_Status eCLD_IdentifyCreateIdentify(
tsZCL_ClusterInstance *psClusterInstance,
bool_t bIsServer,
tsZCL_ClusterDefinition *psClusterDefinition,
void *pvEndPointSharedStructPtr,
uint8 *pu8AttributeControlBits,
tsCLD_IdentifyCustomDataStructure
*psCustomDataStructure);
Description
This function creates an instance of the Identify cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.
The function must be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function creates an Identify cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions.
Note: This function should not be called for an endpoint on which a standard ZigBee device is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function.
When used, this function must be the first Identify cluster function called in the application, and must be called after the stack has been started and after the ZCL has been initialized.
The function requires an array to be declared for internal use, which contains one element (of type uint8) for each attribute of the cluster. The array length should therefore equate to the total number of attributes supported by the Identify cluster. The function initializes the array elements to zero.
Parameters
psClusterInstance: Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initializing individual structure fields.
bIsServer: Type of cluster instance (server or client) to be created:
TRUE - server
FALSE - client
psClusterDefinition: Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the Identify cluster. This parameter can refer to a pre-filled structure called
sCLD_Identifywhich is provided in the Identify.h file.pvEndPointSharedStructPtr: Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type
tsCLD_Identifywhich defines the attributes of Identify cluster. The function initializes the attributes with default values.pu8AttributeControlBits: Pointer to an array of uint8 values, with one element for each attribute in the cluster (see above).
psCustomDataStructure: Pointer to the structure that contains custom data for the Identify cluster (see Section 11.7.1). This structure is used for internal data storage. No knowledge of the fields of this structure is required.
Returns
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_SUCCESS
Parent topic:Functions