Custom Command Responses
The Groups cluster generates responses to certain custom commands. The responses which contain payloads are detailed below:
Add Group Response Payload
typedef struct
{
zenum8 eStatus;
zuint16 u16GroupId;
} tsCLD_Groups_AddGroupResponsePayload;
where:
eStatusis the status (success or failure) of the requested group addition.u16GroupIdis the ID/address of the group to which endpoints were added.
View Group Response Payload
typedef struct
{
zenum8 eStatus;
zuint16 u16GroupId;
tsZCL_CharacterString sGroupName;
} tsCLD_Groups_ViewGroupResponsePayload;
where:
eStatusis the status (success or failure) of the requested operation.u16GroupIdis the ID/address of the group whose name was requested.sGroupNameis the returned name of the specified group.
Get Group Membership Response Payload
typedef struct
{
zuint8 u8Capacity;
zuint8 u8GroupCount;
zint16 *pi16GroupList;
} tsCLD_Groups_GetGroupMembershipResponsePayload;
where:
u8Capacityis the capacity of the Group table of the device to receive more groups - that is, the number of groups that may be added (special values: 0xFE means that at least one additional group may be added, a higher value means that the remaining capacity of the table is unknown).u8GroupCountis the number of groups in the list of the next field.pi16GroupListis a pointer to the returned list of groups from those queried that exist on the device, where each group is represented by its group ID/address.
Remove Group Response Payload
typedef struct
{
zenum8 eStatus;
zuint16 u16GroupId;
} tsCLD_Groups_RemoveGroupResponsePayload;
where:
eStatusis the status (success or failure) of the requested group modification.u16GroupIdis the ID/address of the group from which endpoints were removed.
Parent topic:Structures