Commissioning Commands#
A number of commissioning commands are provided to allow a Commissioning cluster client to remotely request actions relating to the Start-up Parameters attribute set (see Section 43.2.1) on a cluster server. This includes initiating a device restart from the current Start-up Parameter values, as well as the management of these attributes.
Device Start-up#
The ‘current’ set of Start-up Parameter values on a cluster server are those used in the start-up procedure, which can be remotely initiated from a cluster client using the function eCLD_CommissioningCommandRestartDeviceSend(). This function sends a Restart Device command to the remote device hosting the cluster server. This command provides a number of options concerning the timing of the restart:
Without delay: The start-up procedure is invoked as soon as the command is received. This option requires both the delay and jitter to be specified as zero.
**With delay:**The start-up procedure is invoked after a specified delay (in seconds). If no delay is required, the delay period must be specified as zero.
With delay and jitter: The start-up procedure is invoked after a specified delay (in seconds) with a random jitter period added. It is necessary to indicate a maximum jitter period but the actual period will be randomly generated. If no jitter is required, the maximum jitter period must be specified as zero.
Note: If only jitter is required, the delay period must be specified as zero and the maximum jitter period must be non-zero.
In all of the above cases, it is possible to configure the start-up procedure to begin either without any further delay or at a ‘convenient’ moment (when there are no pending actions that should be completed before the restart).
The above options are configured in the command payload (see Section 43.9.2).
The cluster server will send a Restart Device Response to the requesting client before invoking the start-up procedure or starting the countdown (for the delay).
Parent topic:Commissioning Commands
Stored Start-up Parameters#
In addition to the ‘current’ set of values for the Start-up Parameters attribute set, the cluster server can store other sets of values for these attributes in non-volatile memory. Each stored set of Start-up Parameter values is assigned a unique index number. At any time, a particular stored set of values can be retrieved and loaded to become the current set. Functions are provided for managing the saved sets of Start-up Parameter values.
Saving Start-up Parameters#
In order to save a set of Start-up Parameter values, it is first necessary to set them as the current attribute values - this must be done locally by the application on the device hosting the server, possibly using the function eCLD_CommissioningSetAttribute().
The application on a device hosting a cluster client can send a Save Start-up Parameters command to the cluster server in order to request that the current set of Start-up Parameter values is saved to non-volatile memory. This can be done by calling eCLD_CommissioningCommandSaveStartupParamsSend () or, alternatively, eCLD_CommissioningCommandModifyStartupParamsSend (). The index number of the saved record must be specified in the request. If this number has already been used, the existing stored values will be over-written with the new values.
It is the responsibility of the user application on the device hosting the server to perform the save. When the command arrives, a ZCL custom event will be generated and the request should be handled by the user-defined callback function for the endpoint on which the application is located. The server will automatically send a Save Start-up Parameters Response to the requesting client.
Parent topic:Stored Start-up Parameters
Retrieving Stored Start-up Parameters#
A set of Start-up Parameter values that have been stored by in non-volatile memory (as described in Section 43.5.2.1) can be retrieved and loaded as the current set of values. The required stored set of values is specified using its unique index number.
The application on a device hosting a cluster client can send a Restore Start-up Parameters command to the cluster server in order to request that the specified set of Start-up Parameter values is loaded from non-volatile memory. This can be done by calling eCLD_CommissioningCommandRestoreStartupParamsSend () or, alternatively, eCLD_CommissioningCommandModifyStartupParamsSend (). The index number of the relevant set must be specified in the request.
It is the responsibility of the user application on the device hosting the server to retrieve the relevant set of values and load them as the current values. When the command arrives, a ZCL custom event will be generated and the request should be handled by the user-defined callback function for the endpoint on which the application is located. The server will automatically send a Restore Start-up Parameters Response to the requesting client.
A device restart is required in order to implement the loaded values, as described in Section 43.5.1.
Parent topic:Stored Start-up Parameters
Parent topic:Commissioning Commands
Reset Start-up Parameters to Default Values#
A set of Start-up Parameters on the cluster server can be reset to their default values.
The application on a device hosting a cluster client can send a Reset Start-up Parameters command to the cluster server in order to request that the Start-up Parameters are reset to their default values. This can be done by calling eCLD_CommissioningCommandResetStartupParamsSend () or, alternatively, eCLD_CommissioningCommandModifyStartupParamsSend (). Options are available concerning the set(s) of Start-up Parameters to reset - any combination of the following can be performed:
Reset the current set of Start-up Parameters
Reset all stored sets of Start-up Parameters or the stored set with given index
Erase the stored set of Start-up Parameters with given index
The required options must be specified in the request. The option to erase a stored set of Start-up Parameters allows storage space to be freed up.
It is the responsibility of the user application on the device hosting the server to reset the relevant set(s) of values. When the command arrives, a ZCL custom event will be generated and the request should be handled by the user-defined callback function for the endpoint on which the application is located. The server will automatically send a Reset Start-up Parameters Response to the requesting client.
A device restart is required in order to implement the reset (current) values, as described in Section 43.5.1.
Parent topic:Commissioning Commands
Parent topic:Commissioning Cluster