Compile-time options
To enable the Basic cluster in the code to be built, it is necessary to add the following to the zcl_options.h file:
#define CLD_BASIC
In addition, to include the software for a cluster client or server or both, it is necessary to add one or both of the following to the same file:
#define BASIC_CLIENT
#define BASIC_SERVER
The Basic cluster contains macros that may be optionally specified at compile-time by adding some or all of the following lines to the zcl_options.h file.
Optional Attributes
Add this line to enable the optional Application Version attribute:
#define CLD_BAS_ATTR_APPLICATION_VERSION
Add this line to enable the optional Stack Version attribute:
#define CLD_BAS_ATTR_STACK_VERSION
Add this line to enable the optional Hardware Version attribute:
#define CLD_BAS_ATTR_HARDWARE_VERSION
Add this line to enable the optional Manufacturer Name attribute:
#define CLD_BAS_ATTR_MANUFACTURER_NAME
Add this line to enable the optional Model Identifier attribute:
#define CLD_BAS_ATTR_MODEL_IDENTIFIER
Add this line to enable the optional Date Code attribute:
#define CLD_BAS_ATTR_DATE_CODE
Add this line to enable the optional Generic Class Device attribute:
#define CLD_BAS_ATTR_GENERIC_DEVICE_CLASS
Add this line to enable the optional Generic Device Type attribute:
#define CLD_BAS_ATTR_GENERIC_DEVICE_TYPE
Add this line to enable the optional Product Code attribute:
#define CLD_BAS_ATTR_PRODUCT_CODE
Add this line to enable the optional Product URL attribute:
#define CLD_BAS_ATTR_PRODUCT_URL
Add this line to enable the optional Location Description attribute:
#define CLD_BAS_ATTR_LOCATION_DESCRIPTION
Add this line to enable the optional Physical Environment attribute:
#define CLD_BAS_ATTR_PHYSICAL_ENVIRONMENT
Add this line to enable the optional Device Enabled attribute:
#define CLD_BAS_ATTR_DEVICE_ENABLED
Add this line to enable the optional Alarm Mask attribute:
#define CLD_BAS_ATTR_ALARM_MASK
Add this line to enable the optional Disable Local Config attribute:
#define CLD_BAS_ATTR_DISABLE_LOCAL_CONFIG
Add this line to enable the optional Software Build ID attribute:
#define CLD_BAS_ATTR_SW_BUILD_ID
Global Attributes
Add this line to define the value (n) of the Cluster Revision attribute:
#define CLD_BAS_CLUSTER_REVISION <n>
The default value is 1, which corresponds to the revision of the cluster in the ZCL r6 specification (see Section 2.4).
Optional Commands
Add this line to enable the optional Reset To Factory Defaults command on the client and server:
#define CLD_BAS_CMD_RESET_TO_FACTORY_DEFAULTS
Product Code Length
The default length of the product code contained in the attributes sProductCode and au8ProductCode[] can be defined by adding the following line:
#define CLD_BAS_PCODE_SIZE <n>
where <n> is the default number characters in the product code.
The maximum length of the product code contained in the attributes sProductCode and au8ProductCode[] can be defined by adding the following line:
#define CLD_BASIC_MAX_NUMBER_OF_BYTES_PRODUCT_CODE <n>
where <n> is the maximum number characters in the product code.
Product URL Length
The default length of the product URL contained in the attributes sProductURL and au8ProductURL[] can be defined by adding the following line:
#define CLD_BAS_URL_SIZE <n>
where <n> is the default number characters in the product URL.
The maximum length of the product URL contained in the attributes sProductURL and au8ProductURL[] can be defined by adding the following line:
#define CLD_BASIC_MAX_NUMBER_OF_BYTES_PRODUCT_URL <n>
where <n> is the maximum number characters in the product URL.
Parent topic:Basic Cluster