Compile-Time Options#
To enable the Alarms cluster in the code to be built, it is necessary to add the following to the zcl_options.h file:
#define CLD_ALARMS
In addition, to include the software for a cluster client or server or both, it is necessary to add one or both of the following to the same file:
#define ALARMS_CLIENT
#define ALARMS_SERVER
The Alarms cluster contains macros that may be optionally specified at compile time by adding one or more of the following lines to the zcl_options.h file.
To enable the optional Alarm Count attribute, add this line:
#define CLD_ALARMS_ATTR_ALARM_COUNT
To set the maximum number of entries in the Alarms table on the server, add this line:
#define CLD_ALARMS_MAX_NUMBER_OF_ALARMS n
where n is the maximum to be set.
To define the value (n) of the Cluster Revision attribute, add this line:
#define CLD_ALARMS_CLUSTER_REVISION <n>
The default value is 1, which corresponds to the revision of the cluster in the ZCL r6 specification (see Section 2.4).