Supported clusters
The clusters used by the On/Off Light device are listed in the table below.
Table 14. Clusters for On/Off Light |
|
|---|---|
Server (Input) side |
Client (Output) side |
Mandatory |
|
Basic |
|
Identify |
|
On/Off |
|
Scenes |
|
Groups |
|
Optional |
|
Level control |
OTA upgrade |
Touchlink commissioning |
Occupancy sensing |
The mandatory attributes within each cluster for this device type are indicated in the ZigBee Lighting and Occupancy Device Specification (15-0014-01).
Parent topic:On/Off light