MCUXpresso SDK Documentation

BDB_vOutOfBandCommissionGetData

BDB_vOutOfBandCommissionGetData#

void BDB_vOutOfBandCommissionGetData(
BDB_tsOobReadDataToAuthenticate
*psReturnedCommissioningData);

Description#

This function is used to obtain locally stored commissioning data. The obtained data is received in a structure described in BDB_tsOobReadDataToAuthenticate and includes the network key. The data is then passed to higher layers which may encrypt it before sending it by out-of-band means to the other device involved in the commissioning.

A similar set of data but with the network key encrypted can be obtained using the function BDB_eOutOfBandCommissionGetDataEncrypted().

For an overview of out-of-band commissioning, refer to Out-Of-Band Commissioning.

Parameters#

Returns#

  • None

Parent topic:Functions