MCUXpresso SDK Documentation

BDB_teCommissioningStatus

BDB_teCommissioningStatus#

The following enumerations are used to indicate the status of the commissioning process for the node.

typedef enum
{
    E_BDB_COMMISSIONING_STATUS_SUCCESS,
    E_BDB_COMMISSIONING_STATUS_IN_PROGRESS,
    E_BDB_COMMISSIONING_STATUS_NOT_AA_CAPABLE,
    E_BDB_COMMISSIONING_STATUS_NO_NETWORK,
    E_BDB_COMMISSIONING_STATUS_FORMATION_FAILURE,
    E_BDB_COMMISSIONING_STATUS_NO_IDENTIFY_QUERY_RESPONSE,
    E_BDB_COMMISSIONING_STATUS_BINDING_TABLE_FULL,
    E_BDB_COMMISSIONING_STATUS_NO_SCAN_RESPONSE,
    E_BDB_COMMISSIONING_STATUS_NOT_PERMITTED,
    E_BDB_COMMISSIONING_STATUS_TCLK_EX_FAILURE
}BDB_teCommissioningStatus;

The enumerations are listed and described in the table below:

Commissioning Status Enumerations

Enumeration

Description

E_BDB_COMMISSIONING_STATUS_SUCCESS

Commissioning is successfully completed

E_BDB_COMMISSIONING_STATUS_IN_PROGRESS

Commissioning is on-going

E_BDB_COMMISSIONING_STATUS_NOT_AA_CAPABLE

Parent cannot assign address to joining node

E_BDB_COMMISSIONING_STATUS_NO_NETWORK

No network is found that can be joined

E_BDB_COMMISSIONING_STATUS_FORMATION_FAILURE

Network formation failed

E_BDB_COMMISSIONING_STATUS_NO_IDENTIFY_QUERY _ RESPONSE

No responses received to an Identify Query command

E_BDB_COMMISSIONING_STATUS_BINDING_TABLE_FULL

The local Binding table is full

E_BDB_COMMISSIONING_STATUS_NO_SCAN_RESPONSE

No responses received during a channel scan

E_BDB_COMMISSIONING_STATUS_NOT_PERMITTED

Requested commissioning is not permitted

E_BDB_COMMISSIONING_STATUS_TCLK_EX_FAILURE

Trust Centre link key exchange failed

Parent topic:Enumerations